Part Number: TPS48111Q1EVM Hello.
I would like a schematic and artwork (PCB) file of the TPS48111Q1EVM.
I would like to study that board.
If possible, please send it in the comments or one of the emails below.
1. jaeyup7971@naver.com
2. jungjy…
Part Number: TPS48111Q1EVM hello We are designing a power distributor using TPS48111-Q1.
We are currently using multiple TPS48111-Q1 and checking the current value through each Imon pin.
question - Is there a case where the Imon output value is output…
Part Number: TPS48111Q1EVM Other Parts Discussed in Thread: TPS4800-Q1 , TPS4810-Q1 Tool/software: Dear
We are designing for a 55V battery system. I think that TPS48111-Q1 is suitable.
However, we need to withstand a reverse battery connection, upto…
Part Number: TPS48111Q1EVM Hello, I have two questions requested by our customer.
1. What is the maximum allowable current for TPS48111 short circuit protection?
2. Please tell me what is the maximum number of short circuit protection possible…
Part Number: TPS48111Q1EVM Based on the datasheet inrush current limiting depends on the PU resistor & the resistor & cap on the secondary side of PU resistor going to ground (9.3.2.1 on the datasheet). But the EVM doesn't populate all those components…
Part Number: TPS48111Q1EVM Hi Team,
Please confirm whether there is a problem with the test steps: 1. Ground inp and inp_G; 2. Connect to 53.5V DC power supply; 3. Inp pull high to enable, test PU and VOUT
Regards,
Charlie
Part Number: TPS48111Q1EVM Hello Rakesh,
We have used TPS48111Q1 in our BMS system. Yesterday we have tested 5 BMS boards which was finalized in one test setup cell simulator. when we are testing these boards for charge discharge current and short circuit…
Part Number: TPS48111Q1EVM Hello,
I have been trying to drive the capacitive load on the evaluation module with the pre-charge disabled. All the protections have been disabled as well; overcurrent, short circuit, and over temperature. The EN/UVLO is…
Part Number: TPS48111Q1EVM Hi Expert
My customer want to set up the TPS48111EVM.
The Input voltage is 36V, Load current is 2A.
they set the current limit is 15A and disable the precharge function.
EVM can power on that doesn't have any fault when…