Part Number: TPS4813-Q1 Tool/software: Hello — question about the TPS4813-Q1 precharge/LWU behavior (ref: Fig. 7-13 in the datasheet).
If the bypass FETs’ VGS (G2) reaches V_G2_GOOD while the precharge of the load capacitor is still ongoing, and the…
Part Number: TPS4813-Q1 I am designing a BLDC motor control circuit with reverse protected input and load switching using TPS48130QDGXRQ1. The diagram is as shown in the attached image. my design based on the instructions in the schematics (attached image…
Part Number: TPS4813-Q1 Tool/software: Hi Team,
In the TPS4813 we have only one input pin from the microcontroller so can we not control both the channels individually and is there any sequence that the gate driver follows on being enabled like turning…
Part Number: TPS4813-Q1 Tool/software: I am designing a BLDC motor control circuit with protected input and switching using TPS48130QDGXRQ1. The diagram is as shown in the attached image. The Under Voltage lockout, Short-Circuit Protection, Load ON/OFF…
Part Number: TPS4813-Q1 Other Parts Discussed in Thread: BQ76952 , TPS4811-Q1 Tool/software: Hi Team,
I am looking for a gate driver similar to TPS4813 with Vgs protection and current sensing. One criteria being that the current sensing is similar to…
Part Number: TPS4813-Q1 Tool/software: Hello,
I’m planning to use the TPS4813-Q1 in a high-side synchronous switch topology with bypass FETs (G2) and main FETs (G1). I understand the device has VGS comparators for both G2 and G1 and that it checks VGS…
Part Number: TPS4813-Q1 Other Parts Discussed in Thread: TPS2HCS10-Q1 , Tool/software: Is this part number is of ASIL B compliant; if not can you suggest some ASIL B Efuse for a 48V system with SPI communication.
Part Number: TPS4813-Q1 Tool/software: Hi Team,
Could you help to check how to config the G2 if BYPASS is not used? And also about the LFM too.
thanks!
Josh
Part Number: TPS4811-Q1 Other Parts Discussed in Thread: TPS4800-Q1 , TPS4810-Q1 , TPS4813-Q1 , LM74930 , TPS4812-Q1 Tool/software: Hi!
I have a design with multiple TPS48110-Q1.
I want to use it as simple high side switch with 1 MOSFET.
I don…