Part Number: TPS4H160-Q1 Tool/software: Hi TI teams:
I meet a problem about /ST repsonse time.
In TPS4H160-Q1 datasheet, it reocrd the /ST will repsonse after current limit occur.
Is the current limit means the over current occur or thermal shutdown…
Part Number: TPS4H160-Q1 Can the four output channels of TPS4H160 be used in parallel to enhance driving capability? If so, what is the approximate current that can be driven by the four channels in parallel?
Part Number: TPS4H160-Q1 Tool/software: Hi, TI team:
1: We used TPS4H160BQPWPRQ1, the MCU is 5V. but we don't confirm why do we add Rser=10K in the INx signal. Could you tell us the reason?
2: If we used 3.3V MCU, what is the R(ser) value?
3: Do…
Part Number: TPS4H160-Q1 Hi Expert,
Have a nice day.
About TPS4H160-Q1’s inrush current limit function, I can only find limited information in DS. Some questions about this:
1. What is the current level that will trigger inrush current limitation…
Part Number: TPS4H160-Q1
Tool/software:
Hello there,
We take TPS4H160-Q1 chip in our application. when we test EMC-RE item, we found there is an unexpected noise within 300MHz~400MHz as following, it's 5MHz interval. And we located the noise is…
Part Number: TPS4H160-Q1 Are the series current-limiting resistors needed for each of the MCU I/O lines if a free-wheeling diode is used across each inductive load?
Kind regards,
Greg
Part Number: TPS4H160-Q1 Hi,
I am using TPS4H160A-Q1 in our different applications sinse more than 5years and approx >5000 per year.
I am using 4 ICs in one card (i.e. 16 digital output). I got problem in some cards, all output works except when I…
Part Number: TPS4H160-Q1 Tool/software: Hi expert,
Customer inject 12V directly to Outx to drive Relay inductance. When12V inject transient, the waveform is as below and there is a 40V@10ms spike in OUTx pin of TPS4H160-Q1. They also found TPS4H160…
Part Number: TPS4H160-Q1 Tool/software: Greetings
We are performing WCCA on an inverter design which includes TPS4H160-Q1 and while referring the datasheet we didn't find the input current for the below pins.
1. VS (pin 20, 21, 22, 23)
2. SEH (pin…
Part Number: TPS4H160-Q1 Tool/software: Greetings,
We are using TPS4H160-Q1 IC in our design of an inverter. We are using the version B i.e., with SEH, SEL pins.
It is mentioned that the currents from the four channels of the IC gets multiplexed to…