Part Number: TPS51116 Hi Team
do you have any recommendation is 1MHz FSW and 5A output? and other is same function with TPS51116.
Thanks for your help :)
BRs
Brian
Part Number: TPS51116 Can I get a working copy of the PSPICE Model? There was a similar question asked about this on the Power Management Forum.
My simulation just aborts with no errors when I try to run the simulation.
Part Number: TPS51116 I am trying to operate the TPS51116 in current mode control in TINA, but I keep having my output overshoot, trigger OVP, then shutdown.
I am running the output in current mode control at a 1.35V output. The output comes up perfectly…
Hi Timothy,
For EVM access you would need to order one from the TI website. I can use the one I have here and see if I can swap the VDDQSET resistors to make sure the operation doesn't change under this condition.
It sounds like this issue is noise…
Part Number: TPS51116-EP Other Parts Discussed in Thread: TPS51116 I am having an issue with the VDDQ output going over-voltage on startup and not following the Soft-start sequence.
I am currently using the TPS51116 set to a 1.35V output with 6.04k and…
Part Number: TPS51116-EP Other Parts Discussed in Thread: TPS51116 I am seeing a short on my board using the TPS51116 controller between the DRVH and LL pins.
Is this to be expected?
I thought the high-side driver would have a high impedance measurement…
Part Number: TPS51116 Hi BU team,
Can TPS51116 be applied as asynchronous buck? I mean use a diode instead of M2 in the picture below. Thanks.
Regards,
Charlie
Part Number: TPS51116 Hi,
Firstly, I need to say that we already try to simulate many times in pspice and TINA . I am getting error in both simulator and i ask query but i did not got proper answer. Now we try to simulate TPS51116 in LTSPICE, we get error…
Part Number: TPS51116 Hi TI experts,
I recently use TPS5116 to build the buck converter.
and I know this IC is used DCAP approach to compensate the circuit.
and I have some questions about the DCAP, I need some help from TI experts.
in the traditional…