Part Number: TPS51206 Tool/software: Dear Specialists,
My customer is considering TPS51206 and has a question.
I would be grateful if you could advise?
---
Is it acceptable for S3 and S5 to go high either before or after VLDOIN and VDDQSNS rise?
When…
Part Number: TPS51206 Other Parts Discussed in Thread: TPS51200 , Hello,
Our customer is asking that TPS51206 can be used for DDR1 since there is no description with regard to 2.5V VTT supply for DDR1 in the datasheet whereas datashhet of TPS51200 does…
Part Number: TPS51206 Tool/software: Hello team,
TPS51206: has "VLDOIN", "VDDQSNS", and "VDD" as power supplies. Could you please answer the following questions about them?
1. Will the current consumption of "VDD" ever exceed…
Part Number: TPS51206 Other Parts Discussed in Thread: TPS54429 , TPS22959 Tool/software: Please tell me EAR number for below parts.
TPS51206
TPS54429
TPS22959
Hi James,
We just discovered a small defect in the solder paste stencil that caused the reflow process to be faulty.
This seems to be the root cause of the problem.
Thanks for your support.
David
Part Number: TPS51206 Other Parts Discussed in Thread: TPS51200 Hi ,
We are planning to use TPS51206 in our design for powering x8 DDR4 13 Nos.
We have earlier used TPS51200 in other projects for DDR3.
TPS51200 has undervoltage lockout value of min 360mV…
Part Number: TPS51206 Other Parts Discussed in Thread: TMDS64EVM , TPS51200 Hello team,
I am confused on power on sequence of this device.
On datasheet 7.3.6, it says "During power on, it is allowed to turn on VDD, S3 and S5 first, then turn on VLDOIN and…
Part Number: TPS51206 Hello team,
I am confused which configuration I should use.
On 8.2 Typical Application section, there are 2 configurations.
Figure 24 is "VLDOIN = VDDQ Configuration" and Figure 27 is "VLDOIN Separated from VDDQ Configuration"…
Part Number: TPS51206 Dear Tech Support Team,
The customer would like to confirm the date code based on the top markings.
Could you please help to check and advise on the correct date codes? Thanks.
Best Regards,
Dan Lee
Part Number: TPS51206 Hi Team,
The data sheet, 8.2.1.2.5 VTTSNS Connection section, says as bellow. "Consider adding a low-pass R-C filter at the VTTSNS pin in case the ESR of the VTT output capacitor(s) is larger than 2 mΩ.The R-C filter time constant…