Part Number: TPS51275 Other Parts Discussed in Thread: TPS51225 , Hi Sir,
I have some questions of TPS51275 and TPS51225.
1. May I know what's the biggest difference between TPS51225 and TPS51275? I only saw the Vin(min.) and duty cycle are different…
Good Afternoon Scott,
You're correct that the TPS51225's maximum voltage for VIN is 26 V. It's very likely that part is completely dead and could be causing the short. If it is causing the short, and is removed, the TPS25750 would only work in 'Dead Battery…
Part Number: TPS51225
Hi expert,
My customer wants to use 0.22uF as Cboot(Cboot on EVM is 0.1uF). But I didn't see description for Cboot calculation. As I know, risk on larger capacitor is if LS turn on time is enough for charging. Could you kindly help…
Other Parts Discussed in Thread: TPS51225 , TPS54618 Hello,
Do we have TPS54618R and TPS51225 calculator file that can provide to customer? Thank you.
BR
Patrick
Other Parts Discussed in Thread: TPS51225 , TLV320AIC3204 Hell all,
I'm planning to use TPS51225 to convert 7.4V~12V to 5V adn 3.3V.
3.3V will be used for TLV320AIC3204 dsp, but the recommended supply current for this IC was at least 150mA.
In the description…
Part Number: TPS25750 Other Parts Discussed in Thread: BQ25792 , TPS51225 , I have ran into somewhat of a strange problem, and was looking for some input. I have a TPS25750D connected with a bq25792. I had everything working pretty good a few days ago. When…