Part Number: TPS51285B Hi Sir,
Our customer reported that when they are doing the short-circuited testing (Vbus and GND short-circuited) with USB-A interface, that will cause the 5V system power dropout and then the main board to shut down. There is no such…
Part Number: TPS51285B
Hi,TI Team:
A issue about TPS51285B have troubled me for a long time.There is the thing.
When I use the TPS51285B to generate system 3.3V & 5V ,it can work well at some situation,and can pass all the pwoer test like ripple,transeint…
Part Number: TPS51285B Hello Experts, Would you please review a following schematic? https://tidrive.itg.ti.com/a/DrnesoK53qccud6o/7df9fb2a-cc9f-4fda-9540-49dca0deebd8?l Best Regards, Fujiwara
Part Number: TPS51285B Other Parts Discussed in Thread: TPS51225 Hi Team,
There is only the texts description for the Layout Considerations as following in Datasheet. Need your help to check and provide the PCB layout drawing reference design for my customer…
Part Number: TPS51285B Other Parts Discussed in Thread: TPS51285A Hi sir,
The input is 12V, EN1 / EN2 is controlled by LDO3 in my design,
I see that there are some time requirements not specified in the time sequence in the datasheet of Figure 4. TPS51285A…
Part Number: TPS51225B Other Parts Discussed in Thread: TPS51285B , Hi Team,
On ti.com, I see the difference between TPS51225B & TPS51285B as below. Can TPS51225B be used for 5V 20A application? What's the main difference between the two devices. I don…
Part Number: TPS51285B Hi Team,
How much is the PG LOW delay after EN1=EN2=LOW at the same time in TPS51285B? I found the start-up delay is typ. 1.65ms but I couldn't find the low delay.
If possible please give me Min and Max along with the typical…
Part Number: TPS51285B Hi there,
Our customer encountered TPS51285 OCP can only be set to 15A, CS1 and CS2 resistance is 7.5K, And Rds(on)=2.7m omh.
The ocp range can only be 3A~15A.
increase the resistance value OCP can not increase up, but debugging…