Part Number: TPS51312 Hi Team,
Customer would like to design TPS51312. There is no requirement on EN and Vin power sequence.
Customer would like to double confirm the EN and VIN sequence.
Any concern if EN voltage is up before Vin?
Thanks for…
Part Number: TPS51312 Other Parts Discussed in Thread: TIGER , TPS53311 Hi,
TPS51311 mode pin is default set to 57.6K for auto skip mode, is it possible TPS51311 to have force CCM mode setting?
Please advise.
P.S: Because the part number is no…
Part Number: TPS51312 Hello Sir~
I use TPS51312 for 4.2V to 3.33V/2.5A.
0A voltage is 3.339V.
2.5A volage is 3.0682V. (less than spec 3.135V)
Could you have any suggestion?
Thanks.
Part Number: TPS51312 Other Parts Discussed in Thread: TPS53515 Hi Sir
I saw TPS51312 have OCP OVP latch-off function
May I know TI have 8~20A and OCP OVP latch off function solution?
Thanks
Part Number: TPS51312 Hi team,
Can you confirm what is the unit (pF or uF) of CFF in TPS51312 datasheet? The application schematic is show with 47uF, but the table recommends 47pF. If either of them is a typo, please correct it.
Thanks…
Other Parts Discussed in Thread: TPS51312 Hi,
I calculate the value of TPS51312's output capacitors.
The calculation formula is indicated Equation 4 and Equation 5 of Datasheet P12.
I think that As typical calculation formula is L×I(square) = C…
Hi Hardy,
TPS51312 is a possible P2P option for RT8068AZQW. It has similar pin functionalities and uses the same PCB layout.
By the way, you can use the link below for cross reference queries.
Best regards,
Excel
The TPS51396A is functional equivalent to RT6228A, but it is not pin to pin.
TPS51312 for the RT8068A, almost pin to pin, there is a NC pin
RT8816 no equivalent
TPS7A7002 for the RT9059GSP, not pin to pin. no PGOOD