Part Number: TPS51367 Hello,
I'm not able to find the TPS51367 EVM on the web. Is there any way to get something of evaluation kit when we'd like to evaluate it?
Regards, Shinya Sawamoto
Part Number: TPS51367 Hi,
I have created a circuit using the TPS51367 device. Now I am checking the operation of the circuit, but there is concern that the operation of TPS51367 will affect other devices. It is mainly concerning operating frequency…
Part Number: TPS51367 Other Parts Discussed in Thread: TPS51362 , TPS565201
Hi
my current design is 12V to 1.5V, Imax=4A
TPS51367 set Fsw 400khz, inductor is 2.2uH.
is there any solution can let me scale down layout space, thanks
Other Parts Discussed in Thread: TPS51367 Hi Team,
what is the maximum recommended Tjunction for TPS51367? The datasheet only specifies ambient temp. Is it possible to use TPS51367 at higher ambient temps (95°C maybe 100°C) if the junction temperature…
Other Parts Discussed in Thread: TPS51367 Hello
I am question about the TPS51367.
It'll be attached documents about the contents.
Thank you.
TPS51367Q.pdf
Part Number: TPS51367 Hi,
The VSNS pin connects to the load side to use the remote sense function. In this case, I think that it is necessary to connect the GSNS pin to the load side just like the VSNS pin. Is this correct? I am imagining connecting…
Other Parts Discussed in Thread: TPS51367 Hi team,
Could I use to assert EN ,Vin and V5 same timing with TPS51367 ? If could not use same timing , How much time VIN prior asserting EN.
Regards, Kenji Ito
Part Number: TPS51367 Hi,
I am considering a way to supply power to the V5 pin from the outside to reduce device loss. In this case, should we supply low ripple power through the series regulator? Or is it OK with + 5V DC / DC converter (with ripple…
I think that is the trademark name. If TPS51367 does not use that exact technology it is almost identical to it. I could not find any reference to "powerstack" in any of the TPS51367 literature.
Other Parts Discussed in Thread: TPS51367TPS51367 is used in 0.9Vout.
Is the register setting of 0.9Vout right below?
Vout = 2.0 x R1/R1+R2
ex)R1:18kΩ、R2:22kΩ
Best regards,
Satoshi