Part Number: TPS51375 Hi all,
I am asking in this thread because there is no TPS51372RJNR thread.
I am looking for the TPS51372RJNR datasheet. I found the thread requesting 5 years ago, can you share the latest datasheet? I am FAE at TI.
(+) How…
Part Number: TPS51375 Hello,
For a new design, where input voltage is only 12-18V, unregulated, I wonder if connecting directly EN pin to VCC (using internal LDO) will allow the TPS51375 to start (there is no low voltage present before DC-DC has started…
Part Number: TPS51375 Hi,
We would like to request a schematic review for the TPS51375 and other regulators used in our design.
We have a few questions that need clarification to support our layout process and would appreciate your advice.
As this…
Part Number: TPS51375 Hi
I have a question regarding the PATHER LAKE VNNAON RAIL design:
1. Why can I use a TPS51375 12A for +VNNAON 0.77V 26A (but the customer's CPU SKU = 19A)?
Thanks
Part Number: TPS51375 Tool/software: Hi,
The TPS51375 is used to try to achieve the following conditions Vin: 4.5-5.5V Vout: 0.8V Iout: Max. 6A
In WEBENCH Designer the inductor will be 470nH.
However, in the datasheet, 150nH can be used at 0.77V…
Part Number: TPS51375 Dear Sir
I couldn't find the datasheets of below part numbers from your website, could u pls send to me?
TPS51372RJNR, TPS51395PRJER,
TPS51393PRJER,TPS51383RJNR,
TPS51388VABR, TS3USB221RSER,
TPS51488RJER
Ashley
Part Number: TPS51375 Tool/software: Hello SR support team,
This is Dave supporting Industrial PC customers.
We have a new project designing the following spec.:
Vin:4.75V~20V
Vout:0.77V
TDC:7.6A
ICCMAX:15.2A
I found that our new product…
Part Number: TPS51375 Tool/software: Hi,
For pin 7, 13~16, If it's not 'Leave the pin floating or connect to GND' will there be a problem if connected to another power rail? Thanks.
Part Number: TPS51375EVM Tool/software: is there an Altium Design Source file for the Layout Available for the TPS51375EVM ? it's hard to try to track the connections and components on the pictures provided in the user guide..
Thanks