Part Number: TPS513885 Other Parts Discussed in Thread: , TPS51388EVM , TPS51388 Tool/software: this is the schematic
I’m working with the TPS513885VABR buck controller in a design that needs to support input voltages from 5V up to 24V. The circuit…
Part Number: TPS513885 Trying to see what current output I can expect from TPS513885 when routed with 1oz on 6 layers instead of the 4 layer 2oz top and bottom, 1oz internal as recomeded by datasheet. The 1oz assumes using the optional 0.2 vias are placed…
Part Number: TPS513885 Other Parts Discussed in Thread: , TPS51388 Tool/software: TPS513885: No Output Voltage and EN Pin Connected to VCC
Hello,
I use the TPS513885 buck converter in my design to step down 12–24V to 5.15V at 12A. However, I am not…
Part Number: TPS513885 Tool/software: Dear Team,
We are using the TPS513885VABR buck converter in our design, but we are not getting the expected 5V output. We are supplying 12V at 10A to the VIN pin, but there is no output voltage.
We have also tried…
Other Parts Discussed in Thread: TPS51385 Hi TI team,
We’re using the TPS51385VABR to convert a 22V solar input to 5V. With this solar input (open-circuit 22V), the buck fails to start — no 5V output , and the input appears shorted , though there’s…
Part Number: TPS513885 Tool/software: What is the sink current of the Open-drain PG-pin on the TPS513885. - i can't seem to find it in the datasheet. I want to use the PG-pin to drive an LED indicator, without adding an external NFET. Bonus question:…
Part Number: TPS513885 Tool/software: Hi,
We are evaluating the TPS513885 for an upcoming RF test equipment product. Unfortunately we don't have access to PSpice and can't simulate the chip through WEBENCH as simulation is disabled.
Would it be…
Part Number: TPS51388 Hi team,
Customer want to assess Off state power consumption in their system. Would you measure the Iq under below conditions?
Vin=18V, Vout=3.3V with TPS51388 (600kHz, external 5V VCC is applied, Eco-mode)
Vin=18V, Vout…
Part Number: TPS51388 Tool/software: Hello team,
I have been trying to simulate TPS51388/885 using PSpice but load transient simulation is unable in my environment. Could you simulate based on customer's request instead of me?
Followings are the conditions…