Part Number: TPS51396A Hi there,
I have a problem with the IC TPS51396A when I try to power on. There appears to be a short on all pins to gnd (except NC, PGOOD, MODE).
In both cases, there is no load on vout, both boards assembled by JLCPCB.
So…
Part Number: TPS51396A Other Parts Discussed in Thread: TINA-TI Tool/software: Hello, I'm trying to simulate the TPS51396A in TINA-TI. The PSpice model from the website is encrypted ($cdnencstart_adv2 error) and does not work with TINA. Could you please…
Part Number: TPS51396A Tool/software: Hello,
I am experiencing a persistent convergence error while simulating the TPS51396A using PSpice for TI. The simulation runs correctly for a while but consistently fails at T = 6.455 ms with the error ERROR(ORPSIM…
Part Number: TPS51396A Hi Team,
During the OCP test of this VR using TPS51396RJER, we observed that PG is pulled low in the first half of the test and then recovers by itself, as shown in the figure below. Could you please help explain the reason? Thanks…
Part Number: TPS51396A Other Parts Discussed in Thread: TPS51396 Tool/software: Hi,
In our board, we are using the TPS51396ARJET - 5V with 12V input. The output 5v (5V_SW) is coming and goes to power up another section. we design to give the 5VPGOOD…
Part Number: TPS51396A Other Parts Discussed in Thread: LM5148 We mainly have the following two issues that we need your help to take a look at
1. Design requirements: Input voltage 40 to 70V, output voltage 20V, rated output current 15A, peak current…
Part Number: TPS51396A Other Parts Discussed in Thread: TPS74201 , TPS74901 , LM27762 Hello
i am desiging an application where i have 5.5V comming as Vin and i need Vout = 1.0, 1.1, 1.8, 1.9, 3.3 and +/-1.8V. Since it is in instrumentation application…
Part Number: TPS51396A
Tool/software:
Dear TI Engineer,
We cannot find the datasheet of TPS51396RJER on TI website, can you help send it to me?
I found the same post on the e2e forum, but it's been a while and I'm not sure if the methods on…
Part Number: TPS51396A Tool/software: In our design as what shows following, the SW output voltage ranges from -3.5V to 24V.
We try to add snubber, and changes the size (change to 10 ohm & 4.7nf), but the output voltage still ranges from -3.5V to…