Hi Ottey-san,
For the gate driver, I would recommend TPS51604. For the FETs, we have the Power Block II, in a half-bridge configuration, which is 100% lead free with no RoHS exemption. The parts you should consider are the CSD87384M and CSD87588N. The…
Hi Yue,
The Baytrail discrete Reference Designs can be downloaded from the Intel site. In particular, they would want this document: > Intel Baytrail_I Atom E38xx power solutions_May 2016.pdf
as it uses the TPS59641, and as I understand, the SND9039…
Hi Sir,
The Driver is TPS51604.
Please share your mail address for me, we will pass shcematic for you.
if PWM pin pull High 3.4k & Pull Low 1.6K, then Vout is normal.
Do you have any idea for this solution to solve this issue?
Hugo
Part Number: TPS59641 Other Parts Discussed in Thread: TPS51604 , , TPS544C20
Dears,
Customers need V-core solutions based on Inter E3845(X86); 1-phase or 2-phase,15A,
I have recommend TPS544C20/TPS51604/TPS59641,Does TI have full v-core solution…
Part Number: LM5106 Other Parts Discussed in Thread: LM5101A , UCC27712 , TPS28225 , TPS51604 , LM5101B , LM5102 Hi,
my customer is using LM5106 and the drive current is small. They need at least 2A drive current, so I propose LM5101A/B, but this part is much…
Hello John,
I an applications engineer for TI's high power drivers.
I could not find a half-bridge driver with an Iq in the 10uA range but take a look at the TPS51604.
It has an Iq of 160uA (typ) with shoot-through protection inside a WSON …
Other Parts Discussed in Thread: CSD87335Q3D , TPS51604 We use 3-half bridges to drive three phase motor with the configuration:
Driver TPS51604 + CSD87335Q3D
Problem description (the problem occurs only sometimes):
After power switch on the driver…
Other Parts Discussed in Thread: TPS51623 , TPS51604 Dear Sir
I would like to use TPS51623 to design for Vin=24V ,if i change to use TPS51604 , Can I use Vin=24V directly ??
Or I have to transfer the VIn=24V to Vout=12V??
Thanks
Hi John,
Thankw for replaying, in fact there is only tow dual drivers in the website you suggested to me:
1- www.ti.com/.../lm5106.pdf : this driver can drive a half bridge with a maximum input rage of 100V.
2- www.ti.com/.../tps51604-q1.pdf : this…