Part Number: TPS51604-Q1 Other Parts Discussed in Thread: CSD87502Q2 , TPS51604 Hi -
My customer is planning to use TPS51604-Q1 on their new design. This is a battery powered design. Here was the message:
We want to use the TPS51604-Q1 to drive the…
Part Number: TPS51604-Q1 Please tell us the mode transition condition. FCCMVLPM.
In FCCM, /SKIP = H and PWM = L are set.
If /SKIP input voltage is changed from H to 1.6V, will the mode change from FCCM to VLPM?
(PWM remains fixed at L.)
If /SKIP input…
Hi Jerry,
These two devices have different size and EC spec.
Also, TPS51604-Q1 is qualified for automotive application.
I think you can check the spec and pick either one fitting your application.
Thanks
Qian
Hi John,
Thankw for replaying, in fact there is only tow dual drivers in the website you suggested to me:
1- www.ti.com/.../lm5106.pdf : this driver can drive a half bridge with a maximum input rage of 100V.
2- www.ti.com/.../tps51604-q1.pdf :…
Hi Yue,
Apologies, I got confused with these documents. The one you asked for is a TI presentation, attached here.
~Leonard
Intel Baytrail_I Atom E38xx power solutions_May 2016.pdf
Part Number: TPS59641 Other Parts Discussed in Thread: CSD87330Q3D , CSD87334Q3D , Hi sirs,
We test the VCC(Vcore) dynamic VID measurement change Mosfet from csd87330q3d to csd87334q3d
test condition:
Vmax
1.150 V
Vmin
.7 V
…