Part Number: TPS51631A Other Parts Discussed in Thread: TPS53625 Dear Team
Customer would like to select the solution, using for Hewitt lake CPU/VR12.5.
The competitor is NCP81109FMNTXG.
The spec as below :
Input voltage: 12V
Output voltage: 1.05V
Output…
Part Number: TPS51631A Hi team,
Could you kindly give me comment on following customer question?
Q1. Does TPS51631A provide any way to read SVID register without SVID interface accessing from intel CPU?
Best regards,
Takeshi Sasaki
Part Number: TPS51631A Hi,
We have designed TPS51631A and CSD95372 based power circuitry for our custom Intel xeon D processor board.
In order to verify our power circuit, functional simulation model of TPS51631A and CSD95372 is required.
Please share…
Part Number: TPS51631A Other Parts Discussed in Thread: TPS53625 Please we need a clarity on both PMIC's. what is main diff bw both. Why we need to use different PMIC's for D1559 processor core power rails?
Part Number: TPS51631A Hi,
My customer sets the switching frequency setting to 700 MHz.
The waveform of the PWM pin far exceeds the set frequency.
What kind of cause can be considered?
Part Number: TPS51631A We intend to use TPS51631A to convert from 5V to 1.8V.
In the datasheet it is said that conversion voltage range goes from 4.5 to 28V. Regarding VBAT, recommended operating conditions are -0.1V to 28V.
However, there is the following…
Thank you for your answer!
We understood you can't support PMIC for Intel CPU.
Your answer, TPS51631A supports VR12.5.
We are looking for the PMIC that supports VR12 and VR12.5.
Are there PMIC that supports VR12 and VR12.5 other than TPS51631A…