Part Number: TPS51716 Hi Sir,
My customer want use TPS51716 to replace RT8231A for Raptor Lake-U platform core power(1.1V/4.5A), is it suitable?
What is the difference between TPS51716 and RT8231A?
Part Number: TPS51716 TPS 51716 datasheet, 8.2 Typical Application, describes Application Circuits.
Among them, 10 nF (C4) is mounted on the REFIN pin. Could you tell me about it?
1.I want to change the value of 10 nF to 0.22 uF. Is everything all right…
Part Number: TPS51716 Please tell me about switching frequency.
According to the datasheet, 670 kHz operation with Rmode = 12 kΩ. This "670 kHz" is written as Typ.
Please tell me the maximum and minimum frequency when Load Current is 10…
Part Number: TPS51716 I've been trying to simulate our TPS51716 design to get data on the power dissipation but the WEBENCH cannot create a design with Vout < 1.2V. Setting the output voltage to 1.2V or higher seems fine, but with lower voltages…
Part Number: TPS51716 Hello team,
I have a layout review request for TPS51716, can I ask it to your team? I'll send the data offline.
Thanks in advance. S.Sawamoto
Part Number: TPS51716 Hello,
My customer has a question.
Q.
The following description was on the product page of TPS51716.
Iout VDDQ (Max) (A) | 20
Although the TPS 51716 does not have built-in FET, Why are there such restrictions?
Best Regards,
watan…
Part Number: TPS51716 Hi
In the data sheet,
Vref accuracy is described as 8%, but is this accuracy in both PFM / PWM?
Could you tell me please ??
Sincerely