Part Number: TPS53014 Hi,
We got a question from the customer about TPS53014. Could you help us?
[Question] How much is the variation of the Output UVP delay(Tuvpdel)? They don't need guarantee. They will use it as reference.
Best Regards, ta…
Part Number: TPS53014 Hello, We have used this IC to convert 24V DC to 5 V DC.
But it is not working properly. Would it be possible to know what is wrong with our circuit?
We only get about 1~2 V DC output when we put in 24V DC.
Is there any…
Part Number: TPS53014 Hi team,
Can I please understand what causes the maximum output voltage limitation on the TPS53014 and whenever there is anything I could do to use this IC with higher output voltages?
Part Number: TPS53014 Hi,
We got a question from the customer about TPS53014. Could you help us?
[Question] What is the maximum Qg the IC can drive a gate of MOSFET? They are concerned the large Qg will occur a big loss of MOSFET. So they want to…
Part Number: TPS53014 Hi,
We got a question from the customer about TPS53014. Could you help us?
[Question] - Is there any deglitch time on EN function? If 2n to 20nsec very narrow pulse is applied to EN pin, can the IC detect this pulse?
Best Regards…
Part Number: TPS53014 Hi,
We got a question from the customer about TPS53014. Could you help us?
[Question] They are evaluating TPS53014EVM. They found DRVL under-shoot which is over the voltage rating. Please refer to attached file.
TPS53014 DRVL…
Part Number: TPS53014 Hi,
We got a question from customer about TPS53014. Could you help us?
[Question] Our customer is considering using the gate resistor at close to low side FET for protction against under-shoot at DRVL. How much is the recommended…
Part Number: TPS53014 Hi,
We got a question from customer about TPS53014. Could you help us?
[Question] They consider to use TPS53014 under the following condition. How much is the recommended inductance range?
Vin=18.5V Vout=5V Iout=10A
They…
Part Number: TPS53014 Hi All,
I had a question regarding the TPS53014. We're bringing up a board with the device on it to provide 5V, and we can't get it operating properly. Currently, when it's run with no load, the device comes up for a minute or…
Part Number: TPS53014 Hi Expert,
This is a similar question on the thread linked below but target device is different. https://e2e.ti.com/support/power-management/f/196/t/795968
The customer uses TPS53014 to configure a 3.3V Vout buck converter on…