Part Number: TPS53014 Recently when I was looking at this part TPS53014 a question came to my mind ,
Can you please tell me where is the maximum output voltage as specified in the data sheet coming from ,
I can see the output voltage is 7V ,
I was wondering…
Part Number: TPS53014 Hi All,
I had a question regarding the TPS53014. We're bringing up a board with the device on it to provide 5V, and we can't get it operating properly. Currently, when it's run with no load, the device comes up for a minute…
Part Number: TPS563209 Other Parts Discussed in Thread: TPS53014 , TPS54320 , TPS54620 Hi
My customer use TPS563209 and TPS53014.
These two devices are described as follows about Cout.
But they demand large capacitor for high-quality sound.
How much capacity…
Other Parts Discussed in Thread: TPS53014 Hi,
My customer has question about TPS53014. Could you tell me about questoin?
[Question] - How much is the recommended range of the bootstarp capacitor? Could you tell us the concern if the bootstarp capacitor is…
Dear Qian Chen,
May I ask a qestion about UVP?
Could the output voltage recover during the UVP delay time?
My customer says although the output voltage is restoring during the delay time, Is TPS53014 such behavior?
Best regard, Bob Lee.
Other Parts Discussed in Thread: TPS53014 Hi,
My customer has question about TPS53014. Could you tell me about questoin?
[Question] - How much is the recommended range of soft-start capacitor(Css)? My customer considers to use 4.7nF to 6.8nF. Is there any…
Other Parts Discussed in Thread: TPS53014 , TPS53318 , LM5117 Hi,
Customer of mine is seeking to DCDC for TV application with the specs below:
Vmax Input = 22V
Vout = 1.0~1.1V
Iou = 8A or higher ..
(ECO mode , Over/Under voltage protection , and other unique…
Other Parts Discussed in Thread: TPS53014 Hi,
My customer has question about TPS53014. Could you tell me about questoin?
[Question] - What is UVP Reset Condition? Is it only when EN goes Low? Is it reset when VREG5 voltage reaches UVLO?
Best Regards, tat…
Other Parts Discussed in Thread: TPS53014 Hi Team,
I am fine tuning the TPS53014 EVM for a specific output conditions. Can you please explain why and how values of R5, R7 and R10 were picked?
Best regards,
Rohit Joshi
Other Parts Discussed in Thread: TPS53014 Dear support member,
TPS53014 evaluation board ENA pin has connected to GND with 1kΩ. If ENA pin has connected to directly GND with MOSFET,It will not be a problem?
Could you checked of attached file?
Best…