Part Number: TPS53015 Hey, had a question about the PG pin on TPS53015. I am a bit confused how PG is an open drain output pin, but in 7.2 (functional block diagram) it looks like it is actually attached to the gate of a MOSFET between the feedback comparators…
Part Number: TPS53015 Other Parts Discussed in Thread: CSD87350Q5D , , SYNC-BUCK-FET-LOSS-CALC , TPS40050 , LM3150 Hi TI,
I'm seeking for alternate part for the switching controller TPS53015DGS , I had designed the part for below mentioned configuration…
Part Number: TPS53015 Other Parts Discussed in Thread: TPS53014 Hi,
I am using TPS53015 Buck regulator in my design. But due to the lack of parts I am planning to replace TPS53015 with the TPS53014 part from TI. While comparing the datasheet the pin 2…
Part Number: TPS53015
Hi,
Please review the attached schematics and let me know your valuable comments.
Vin = 24V normally Vout = 5V, 12A
Please review specially the feed back resistors and Inductor calculation.
I am little bit confused about the inductor…
Part Number: TPS53015 Dear sir,
Please help to check if my TPS53015 design is ok, thanks!
I already tested the output voltage, found that the maximum overshoot is about 30mV, how can i fix this issue?
Part Number: TPS53015 Other Parts Discussed in Thread: , TPS51215A , TPS51916 Hi, support team
My customer has the questions as follow:
There's an D1 BAT54XV2T1 in TPS53015EVM-126. According to the follow post, I know that it clamps the negative voltage…
Part Number: TPS53015
During load, test found a dip(2.5 v old glitch found during the 5-ohm loading) on the 5V while loaded with 5ohms. Kindly check it and inform me what is the reason for the dip.
Inductor Value: 2.2uH and output cap is 220uF.
Part Number: TPS53015 I am simulating the part number above in PSpice for TI. The simulation runs fine, but I'm attempting to simulate the effect of saturation current on the inductor. How can I enter my desired value for saturation current? Also related…
Part Number: TPS53015 Other Parts Discussed in Thread: TPSM5D1806 , TPS543620 Hello,
I'm using the TPS53015 device as a step-down converter to generate 5V out of a battery. I would like to guarantee that the device will not be damaged or will not generate…
Part Number: TPS53015 Other Parts Discussed in Thread: CSD86350Q5D
Hi,
I am trying to use TPS53015 for converting 19V input to 5V output at 10A current requirement. Since TPS53015 is a buck controller, I chose a MOSFET of this part number "CSD86350Q5D…