Part Number: TPS53119 Tool/software: hi,
The schematic diagram of TPS53119 is shown below, with an input voltage of 12V, an output voltage of 1.8V, and a maximum output current of 10A. Please help check if there are any issues with the schematic diagram…
Part Number: TPS53119 Other Parts Discussed in Thread: CSD86350Q5D
Hi TI Team, I Thought of using TPS53119 in one of my project, where my requirement is Vin : 12VDC (Nominal), Vout : 0.8V, Iout : 20.6Amp(Nominal) & 22Amp(Max). I had simulated the same…
Part Number: TPS53119 Hi,
I am having trouble getting the expected voltage from the PGOOD pin when the TPS53119 is done starting up.
Below is a screenshot of part of my schematic:
R52 sets the soft-start time, along with R47 I am expecting PGOOD to…
Part Number: TPS53119 Tool/software: WEBENCH® Design Tools How does the Webench tool calculate the value for the Rtrip resistor and the resulting Iocp values? Calculating the Iocp value with the Rtrip resistor value from Webench based on the datasheet…
Part Number: TPS53119 Hi team
My customer want to change the IC from RT8237FGQW to TPS53119RGTR.
I want to change the IC that is applied to Intel CPU EVM.
Is there a problem when I change it?
Thank you.
Hello,
TI offers a variety of buck controllers that may work in place of the TPS53015DGS.
As a drop-in replacement (without adjustable soft-start), I would recommend the TPS53014- https://www.ti.com/product/TPS53014
If a DCAP/DCAP2 topology is desired…