Part Number: PSPICE-FOR-TI I just downloaded the simulation model from following link.
TPS53313 Unencrypted PSpice Transient Model Package (Rev. A) — SLUM254A.ZIP (51KB)
I keep getting error message "ERROR(ORCAP-15053): Can not initialize PSpice UI…
Part Number: TPS53313 I have been learning voltage mode control of Buck recently, and I am study how the transient response is influenced by the crossover frequency. I find many materials tell that the oscillation frequency of transient voltage in closed…
Part Number: TPS53313 Other Parts Discussed in Thread: TPS53312 , TPS54326 Hi
when I use TPS5331 2 , (I can not find TPS53312 in Part number)
when the system have abnormal voltage on "Sw" pin, it causes leakage on "Vin " pin .
how to…
Part Number: TPS53313 According to datasheet, TPS53313RGER has 24 pins. But the sch/pcb symbol downloaded from here, only has 20 pins.
vendor.ultralibrarian.com/.../embedded
Part Number: TPS53313 Hi,
I have made 5V, 6A output current switch circuit using TPS53313. I have followed G3-PLC (CENELEC Band) Data Concentrator Reference Design page #47.
Now when I test using 1 ohm, 5w or 10w resistor it gives maximum 5V, 2A power…
Part Number: TPS53313 Other Parts Discussed in Thread: TINA-TI hello! i want to set TPS53313 to operate in forced ccm mode. i have some questions regarding this mode: 1) is there any minimum load requirements? 2) the current of the inductor starts at zero…
Part Number: TPS53313 Other Parts Discussed in Thread: TPS53315 , TINA-TI Tool/software: WEBENCH® Design Tools I would like to report TPS53313 webench tool issue.
customer reported the Webench tools does not have “run simulation” icon on TPS53313…
Part Number: TPS53313 Dear sir:
I found problem with following circuit when the initial current load is ~1A. current load is permanently connected at output.
When VOUT_EN is on, the vout is 4V which generate 1A on 4ohm load. The hiccup occurs as below…
Part Number: TMS320C6657 Other Parts Discussed in Thread: TPS53313 , LM10011 , TPS54424 , I'm looking at various different Power Supply options for the C6657 implementation. I've been told that the Smart Reflex feature is not optional for the Keystone I device…
Other Parts Discussed in Thread: TPS53313 E2e,
Our customer needs the logic threshold levels for the TPS53313 RT/SYNC pin. We don't see this information in the data sheet. Can you help please?
Thanks for your help.
Regards,
WH