Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS53315 Dear Team,
Do we have any solution can meet the spec below?
Vin =4.1V (max)
Vout =2.3V
Iout =12A (max)
Auto Grade AEC-Q100
Many Thanks
Jimmy
Part Number: TPS53315 Hi,
could you please let me know for GND1 pin of TPS53315 is there any consideration need to be taken in schematic and layout like separate signal gnd(analog gnd) ?
and is there any special consideration for GND2 pin?
thanks and…
Part Number: TPS53315 Other Parts Discussed in Thread: TPS25982 , TPS22959 Hi,
Attached is my current schematics for TPS53315. My Vin=12V, Vout=5V and Iout=12A.
I am currently facing power fluctuation issue during SATA HDD hotplug which has 5V connected…
Part Number: TPS53315 Other Parts Discussed in Thread: TPS548A20 , TPS25982
Hi ,
I am using TPS53315 in my design. I sharing the webench simulation that I used to check my design here.
webench.ti.com/.../114
Vin=12V, Vout=5V, Iout=8A, fsw=500kHz, SS…
Part Number: TPS53315 Tool/software: WEBENCH® Design Tools hi,
i have shared My WEBENCH TPS53315 design publicly, beow is the link.
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=8E9069BE200976FA
OUTPUT -5V , INPUT -12V, OUTPUT CURRENT -11A…
Part Number: TPS53315 Tool/software: WEBENCH® Design Tools hi,
i have shared my WEBENCH design below
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=8E9069BE200976FA
OUTPUT -5V , INPUT -12V, OUTPUT CURRENT -11A, FSW 500KHz
in my ckt
L1- XAL7070…
Part Number: TPS53315 Tool/software: WEBENCH® Design Tools Hi,
I am not getting current waveform while doing load transient simulation for TPS53315, is that option is not available.
Also please let me know how to set lower and upper current values…
Part Number: TPS53315 Tool/software: WEBENCH® Design Tools hi,
i am using TPS53315 in my design below are the few queries related to its simulation.
Please find the below ripple waveform, steady state simulation result of TPS53315 using WEBENCH design…
Part Number: TPS53315 Tool/software: WEBENCH® Design Tools hi,
1) In TPS53315 data sheet soft start timing selection range is 0.7ms to 5.6ms but in WEBENCH design tool it is from 3- 10 ms and also that option is not working.
2) Why Mode selection option…