The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: TPS53317A Tool/software: ATTENTION: This is the ONLY attempt by IBM to secure information regarding the use of the newly added SVHC(s) in deliverables supplied by your company to IBM. If no response is received, IBM interprets your silence…
Part Number: TPS53317A Tool/software: The TPS53317A on a new board design no longer has a voltage output after initially working.
I have a brand new board design which uses the TPS53317A to supply 0.72V to an FPGA. Vin is 1.2V. Upon power up of the board…
Part Number: TPS53317A
Hi:
Why we should place a 10 ohm resistor with a 0.1 uF capcitor from the output to the VOUT Pin? Can I change the RC value to 1 ohm and 0.01 uF?
Thanks!
Jiajun
Part Number: TPS53317A
Hi All,
May I know what is the frequency tolerance under 1.2V input, 0.6V output, 2.7A Iout, and 600kHz setting?
It hard to judge based on the below figure from the datasheet.
The customer request +/-10% means 540KHz~660kHz but…
Part Number: TPS53317A Hi team,
My customer is using the TPS53317A now.( non-tracking mode). The start up waveform is as below which is not monotonous. Do we have some suggestions to improve it? i have suggested the customer to add more output cap 2*470uF…
Shuang Feng76,
There are multiple layers to the device. The changes described between the TPS53317 and the TPS53317A are minimal, so these changes may not be present in the top layer.
Thanks,
Kadeem
Part Number: TPS53317A Hi team,
The operating temperature range of TPS53317A shown on the webpage is -40~125℃, but in the datasheet is -40~85℃,which is the ture operating temperature range?
Part Number: TPS53317A hello
I am using the TPS53317A VR in a tracking configuration.
I have a digital Potentiometer that is connected between Vref pin and Refin pin and controls the voltage divider between those pins.
when I change the voltage in the…