Part Number: TPS53317A Hello,
Posting on behalf of my customer.
Based on the package options in the datasheet, the TPS53317A is rated up to 125C operating temp. However, when creating a new design in Webench Designer it limits me to 85C so I cannot check…
Part Number: TPS53317 Hi Team,
As TPS53317 and TPS53317A are pin-to-pin compatible devices, I'd like to know if they are also BOM-to-BOM compatible?
In other words, do we need to change anything in the schematic when switching from TPS53317 to TPS53317A…
Part Number: TPS53317A Other Parts Discussed in Thread: TL431 , Hi,
I have created a circuit to power SSLT2 using TPS 53317A. My circuit has problems. Since the DCDC Buck on the input side of TPS 53317 A can not be sink, the input voltage (2.5 V) of TSP 53317…
Other Parts Discussed in Thread: TPS51200 , TPS51206 , TPS53317A 4118.DDR3.pdf
Hi Team,
My customer is using Intel Cyclone 10GX FPGA to interface with Micron 2Gb DDR3 memory is attached. DDR3 ip core inside FPGA operating frequency is 200MHz in our design…
Hi Peter
I would like to ask another question regarding to noise in the power good signal.
I tried to measure the power good signal in TPS53317A (FET-integrated) with setup limit probe bandwidth at 250Mhz but I did not see any noise in this signal. Could…
Hi Charles,
If the max VTT current is 3A, I would suggest to use switching converter TPS53317A for VTT rail.
The TPS51116 VTT regulation may not be good at 3A load.
Thanks
Qian