Part Number: TPS53318 Hello Team,
My customer would like to know if running the TPS53318 in FCCM mode offer a faster transient response compared to Skip mode? They have an application that could demand up to 3A@3.3V with a slew rate of 1A/us.
Thanks in…
Part Number: TPS53318 Other Parts Discussed in Thread: TPS53319 , Dear Team,
My customer has used TPS53318 and TPS53319 at their products since 2019. They designed their application circuit based on Rev.E datasheet of TPS5331x (SLUSAY8E). They leave ROVP…
Part Number: TPS53318 Design parameters: Vin : 5V ,Vout : 4.2V and Iout 3A.
Observation:
At 0.3A Load, the output voltage obtained as 4.13V, Duty Cycle - 87.33% , Vfb - 0.62V
At 3A Load , The output voltage obtained as 3.86V, Duty Cycle - 78% , Vfb-0…
Part Number: TPS53318 Hi support team,
Floating ROVP pin has been prohibited from SLUSAY8F. Please let me know the reason.
Is it because the 1.5MΩ pull-down resistor has small current and noisy?
Regards, Dice-K
Part Number: TPS53318 There are already several posts about this issue which where closed without any answer.
Can please somebody tell me the RDS(on) or tell me why it is not specified in the data sheet?
Part Number: TPS53318 Tool/software: WEBENCH® Design Tools Hi,
I have used Webbench power designer to design a 5V regulator using the TPS53318 part. Schematic is attached.
I have looked at all of the voltages on the board an all look correct, but the…
Part Number: TPS53355 Other Parts Discussed in Thread: TPS53319 , TPS53318 Hello expert,
Customer would like to achieve co-layout design for TPS533XX. As checked with datasheet, the difference between TPS533XX series is ROVP. May I know if we can connect…
Part Number: TPS53318 Hi Expert,
The customer see the TPS53318 is running the 1.2M within the 750Khz setting at their board.
The captured waveforms as below:
Within different the output current, this situation still keep the same.
The RD want to know…