Part Number: TPS53318 Other Parts Discussed in Thread: TPS53319 , Hello team,
Our customer is planning to replace TPS53318 for delivery issue, and assumed if TPS53319 could be considered as an alternative. As far as I saw the datasheet, the only difference…
Part Number: TPS53319 Hi support team.
I received a inquiry from my customer.
Is it permissible to apply voltage from an external circuit to the VREG pin when VDD=0V?
A voltage (3.3V) is applied to the VREG pin before the device starts up (VDD=0V…
Part Number: TPS53319 Hello,
My customer is using TPS53319 for their design. After power up, their load current starts increase intermittently. Then some TPS53319 (they call this good device) work correctly, but some TPS53319 (they call this NG device…
Part Number: TPS53355 Other Parts Discussed in Thread: TPS53319 , , TPS53353 Hi Team,
Customer wants to use TPS53355 to replace TPS53319 in their board because of device shortage. I check both D/S, these footprints are same. Do you think are there peripheral…
Part Number: TPS53319 Other Parts Discussed in Thread: TPS548A28 , TPS53318 I need some help finding a replacement part for TPS53319DQPR.
Do we have anything P2P that can be used here with similar or better functionality?
Hi Albert,
Could you please let us know your input/output [Vin = ??, Iout=10A, number of series LEDs = ??, Forward voltage of each LED = ??] requirements to supply an LED so that we can assist you for your application ?
Also, TPS53319 is a voltage…
Part Number: TPS53319 Hello,
My customer designed Vin=12V, Vout=3.3V and Iout(max)=8A buck converter circuit using TPS53319.
Please review their schematics and provide feedbacks. tidrive.itg.ti.com/.../e6926fb2-d9ff-4854-9b3f-08ff68b4de19
Best…
Part Number: TPS53319
Hi
I use TPS5 3319 for my VRM to design. I want to make loop statility test on TPS53319. There is some info on page 7 of the datasheet about the application circuit diagarm, but the test point about the loop stability test is…
Part Number: TPS53319 Hi,
could you provide the low sdie Rds(on) for me? i would like to calculate the OCP but i can't find this pararmeter on datasheet.
thx.
Part Number: TPS53319 Hi
I got a question from my customer about Vreg capacitor of TPS53319.
This device is used Vreg capacitor of 1uF in typical application.
Could I use the capacitor of 10uF?
Best regards,
Yokota