Part Number: TPS53321 Other Parts Discussed in Thread: TPS62867 Hi, I do not see TPS53321 in TI pspice. Is there a similar part that is available in TI pspice that can be used to verify the TPS53321? Transient is preferred but I can use average if it…
Part Number: TPS53321 Other Parts Discussed in Thread: TPS62866 , TPS62869 , TPS54478 , TPS62826A Hi sirs,
My customer would like to estimate TPS53321 efficiency, however, only high/low side Rds_on on data sheet. This device is not in Webench. Is there…
Part Number: TPS53321 Other Parts Discussed in Thread: TPS62867 , TPSM82866A Hi,
What should be the connections with SYNC pin when I want to use only one regulator (TPS53321). Means there is any Slave or other regulator to receive that synchronization…
Part Number: TPS53321 Other Parts Discussed in Thread: TPS53311 , TPS53310 , TPS62867 Dear All
1. Do TPS53321(5A), TPS53310(3A), TPS53311(3A), VDD 12 PIN and VIN 13 PIN need power sequence?
2. TPS53321(5A), TPS53310(3A), TPS53311(3A) , SYNC 2 PIN…
Part Number: TPS53321 Other Parts Discussed in Thread: TPS53311 , TPS53310 , TPS62867
Dear All
May I ask if TPS53321(5A), TPS53310(3A), TPS53311(3A) are pin to pin with NCP3135(5A)?
Part Number: TPS53321 Other Parts Discussed in Thread: TPS62867 , TPSM82866A Hi,
In the datasheet, Figure 13. Typical 3.3-V Input Application Circuit Diagram shows R6 connected to the VDD pin and VIN pin, but since the datasheet does not specify the…
Part Number: TPS53321 Hi,
I check datasheet and the device support input voltage range is 4.5~18V.
My customer design is output voltage=1.8V, the input voltage=4.5V is ok for the design, right?
The other question is the device has max duty cycle…
Part Number: TPS53321 Hi,
I need to now how must current the internal LDO require during normal operation and at startup.
The only information the datasheet contains are information about shutdown current IDDSDN = 5uA and standby current IDD = 2…