Part Number: TPS53513 Tool/software: Hi
I have been reviewing the TPS53513 datasheet and would like to clarify the EN-to-VOUT startup time. According to Section 7.3.2 and Figure 33 (Power-up Sequence Waveforms), When the EN pin voltage rises above…
Part Number: TPS53513 Tool/software: Hello
Can you please review the schematic diagram LAYOUT? tks! RIO card schematic_TI_20250513.pdf TPS53513_RIO card_25250513.pdf
Part Number: TPS53513 Do we have any guidance on the distribution of soft-start time for this device (from the rise of EN)? Esp. the Max time.
We have a system that requires the device to reach regulation within 2.2msec and need to know if this device…
Part Number: TPS53513 While testing start-up sequence in our design, I observed about 1ms of delay between enable and soft-start. A diagram in datasheet shows that the delay is about 400 µs. However there is also a start-up sequence waveform in datasheet…
Part Number: TPS53513 Hello.
I'm now trying to make 0.9V using TPS53513. So I have a few questions. It generates 0.9V from 12V, but 12V has switching noise of about 100kHz.
Is the only way to reduce this noise is to filter the input stage of the TPS53513…
Part Number: TPS53513 Hi,
We are assessing the failure mode of the converter design. We would like to know if OCP threshold will change when TRIP pin is shorted to GND or floated while the converter is running.
From the datasheet I'm assuming the…
Part Number: TPS53513 Hi All,
A customer using TPS53513 reported an abnormal output voltage. I want to send a waveform, but I haven't got permission from the customer, so I want to share it via private message or email.
We look forward to your support…
Part Number: TPS53513 Dear Team,
The customer has a board with 53313, and now encounters the problem of sending PGs out, this group of PGs is sent to CPLD. I would like to ask, VREG also has 5V, EN those are normal ~ output also has normal output of…
Part Number: TPS53513 Hi,
I can't find VIN-SW (HS FET Vds) spec in datasheet.
Do we spec the max voltage rating?
My customer measured -6.72 negative voltage on VIN-SW, is that OK?