Part Number: TPS53513 Hi,
I can't find VIN-SW (HS FET Vds) spec in datasheet.
Do we spec the max voltage rating?
My customer measured -6.72 negative voltage on VIN-SW, is that OK?
Part Number: TPS53513 Other Parts Discussed in Thread: TPS53915 , I would like to make a design to place either the TPS53915 or the TPS53513.
Question abotu pins 27 & 28 when using the TPS53513 - if these are connected to I2C pins of a micro or FPGA…
Part Number: TPS53513 Hi,
In page #16 of data sheet, Figure 33 shows that enable pin should be asserted after VDD is stable.
Is this a requirement to make TPS53512 works? I am using a resistor divider on enable pin from other power regulator,
The…
Part Number: TPS53513 Hello,
We've been using the TPS53513 on one of our product for a couple of years without any problem but on the last batch Vout happens to be out of spec.
When the board is idle (low power), we measure FB at 0.6247 V and 0.6272…
Part Number: TPS53513 Other Parts Discussed in Thread: TPS53515 , , TPS548A20 , TPS53915
The TPS53515 is in FCCM when the mode pin is connected to either PGOOD or VREG. What is the minimum voltage requirement for connecting the mode pin to PGOOD?
…
Part Number: TPS53513
Is it possible that there are diffferent Xray images of PN:TPS53513RVER( see attached jpg) because of different DC or any other reasons?
For infomation , the CSO/CCO , ASO ACO are the same except the different DC
Part Number: TPS53513 Hi All,
I have a question about TPS53513.
The customer performed an IV evaluation of the SW terminal and the PGND terminal using two samples of good. The result is as follows.
Results will vary depending on the sample.…
Part Number: TPS53513 Hi Team,
For TPS53513, the thermal shutdown temp is 140C and hysteresis is 40C. Does it mean it will resume to work when Tj drops to 100C? This is a very high hysteresis.
Regards,
RJ
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS53513 Hi All,
I simulated TPS53513 with webench, but there was no phase margin result. Is it possible to simulate the phase margin?
Best Regards, Ishiwata
Part Number: TPS53513 Hi Team
Could you tell me the process capability of TPS53513RVER,my customer want to know how much "nm" of the chip, I see the website ,but it show "MULTIPLE", so could you tell me the meaning of MULTIPLE, 350nm or 400nm ?
…