The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: TPS53513 Hi,
In page #16 of data sheet, Figure 33 shows that enable pin should be asserted after VDD is stable.
Is this a requirement to make TPS53512 works? I am using a resistor divider on enable pin from other power regulator,
The enable…
Part Number: TPS53513
Hi team,
I would like to double confirm TPS53513 UVP/OVP/OCP are all latch mode, and can only be recovered by recycling VDD or EN, correct?
Thank you.
Regards,
Allen
Part Number: TPS53513 I want to know the variation of switching frequency.
Could you tell me the precision (e.x. ±10%) or measured distribution data of switching frequency?
Part Number: TPS53513 Hi Sir,
TPS53513 in the design as below:
Vin=12V Vout=0.95V Fsw=500KHz L=1uH Iload=6.4A
Jitter is 28%, over 20%, could you give some suggestions on this?
Thank you.
Part Number: TPS53513 Other Parts Discussed in Thread: TPS54824 Hi Sir,
Coulde I use TPS53513 in the applacation as below:
Vin=5V Vout=4V Iout=3.5A
The concern is could TPS53513 handle the big duty cycle? the worst case should be at the start up.
and…
Part Number: TPS53513 Other Parts Discussed in Thread: TPS53313 Hi!
my customer wants to use TPS53513, but this note in the datasheet is not clear:
Is this network required for the TPS53513? If yes, which values do you recommend?
Kind regards,
Mar…
Part Number: TPS53513 Hello E2E,
If PGood is not used, can it be left floating? Section 7.3.5 states that it must be pulled up externally, but is that just if it is needed?
Thanks!
Russell