Part Number: TPS53513 Hello E2E,
If PGood is not used, can it be left floating? Section 7.3.5 states that it must be pulled up externally, but is that just if it is needed?
Thanks!
Russell
Part Number: TPS53513 Other Parts Discussed in Thread: TPS54824 Hi Sir,
Coulde I use TPS53513 in the applacation as below:
Vin=5V Vout=4V Iout=3.5A
The concern is could TPS53513 handle the big duty cycle? the worst case should be at the start up…
Part Number: TPS53513 Other Parts Discussed in Thread: TPS53313 Hi!
my customer wants to use TPS53513, but this note in the datasheet is not clear:
Is this network required for the TPS53513? If yes, which values do you recommend?
Kind regards…
Part Number: TPS53513 Hi,
May I know the epoxy voids criteria for the device TPS53513 (VQFN-CLIP).
Hope i could get some information about this, thank you!
Part Number: TPS53513 Hi, Could you tell me about "tOVPDLY" test condition written in datasheet P.7? TEST CONDITION says "With 100-mV overdrive", What condition does it mean? Best regards, Yuto Sakai
Part Number: TPS53513 Other Parts Discussed in Thread: TPS563210A , Hi Team,
Can I kindly ask for the efficiency between TPS53513 and TPS563210A under condition of 12Vin/5Vout@0~3A ,
my customer is choosing TPS53513 as solution seems their application…
malli,
I suppose can contact your local sales office. I cannot really comment about how support works in India.
TPS53513 is designed to operate in FCCM mode. In FCCM, there will be negative switch current when Iout is less than ILp-p/2. There is no…
Part Number: TPS53513 Other Parts Discussed in Thread: TPS548A20 TPS53513 has two MODE resistor value depend on R-C Time constant.
Skip mode: 0k ohm and 150k ohm
FCCM mode: 20k ohm and 150k ohm
How can we select these resistor value? Which case…