Part Number: TPS53622 Hi team,
My customers measured the SW waveform of TPS53622, didn't connect CPU load.
They found the actual SW frequency is only 556kHz, lower than the setting value 800kHz. They also measured other rails, the frequency was setting…
Part Number: TPS53622 Other Parts Discussed in Thread: CSD97374Q4M , CSD97370Q5M , PMP21872 , , TPS53676 , TPS53681 Dear Team,
I am planning to use Buck Controller TPS53622RSBR with the power stage of CSD97374Q4M or CSD97370Q5M for a dual-phase buck converter solution…
Part Number: TPS53622 Other Parts Discussed in Thread: TPS53679 , Hi all,
I need to know if the Pinout of the PNs: TPS53679RSB, TPS53679RSBR, TPS53659RSBT and TPS53659RSBR are compatible or close to the TPS53622RSBR.
Thank you
Part Number: TPS53622 Hello,
I am aware that the main difference with the TPS53622A is the added ability to program the OVP threshold to 200mV or 400mV. From that, I am confident the A-part would work just fine in a system designed with the non-A-part…
Part Number: TPS53622 Other Parts Discussed in Thread: TPS53679 Hi team,
My customers are using TPS53622 and SN1701022.
They found a problem that VR turn-off time is too long (200~300ms), even though they add the discharging resistor 100ohm parallel with…
Part Number: USB-TO-GPIO2 Other Parts Discussed in Thread: TPS53659 , TPS53622 , Tool/software: Hi,
We have used the multiphase VR ( P/N: TPS53659 and TPS53622 ) on our custom board.
Now, to program/ configure the VR, we need a USB Interface adaptor.
I want…
Part Number: TPS53622 Hi SIR
Our product is designed with Intel CPU and matched with TPS53622 power supply. The circuit and Bode plot and POL Transient diagrams and specifications are as follows~~
Input : 12V
Output : 1.82V (two phase)
Iout : 55A
Fsw…
Part Number: TPS53622 Other Parts Discussed in Thread: TPS53625 , Hi all, My customer needs to build a power stage system for an Atom Intel C3000. At first the system was made up by: TPS53625 + CSD97370; with a 18V supply. --> unsatisfactory results. The new…
Part Number: TPS53622 Other Parts Discussed in Thread: CSD95496QVM , Hi,
We are using TPS53622A+CSD95496QVM*2, Just want to make sure is there anything need to pay attention if switching Vin from 12V to 5V?
And the output should be 0.72V, 40A.
Per our datasheet…
Hello Chasel,
I know the reason. TPS53622 always regulates the voltage across VSP-VSN=vboot,but intel PCH will read the PVNN-GND.
Attachment is TI reference design.,in the SCH the voltage across PVNN_P-PVNN_N is always =vboot, but the PVNN-GND will over…