Part Number: TPS53625 The layout recommendation figure 60 in the data sheet shows feedback and bias being routed to Vout using two separate connections. I'm using a fixed 3.3V version.
1. If there is a 3.3V (VOUT) plane in the PCB is it OK to connect…
Other Parts Discussed in Thread: TPS53625 Hi
Recently I used TPS53625 as my x86(ATOM C3000) CPU VR chip. I set the TPS53625 min Vcs(ocp) value to 4.5mV. When I run linux on the CPU.I found the running speed is very slow. I use dd command the write sata…
Other Parts Discussed in Thread: TPS54625 , TPS53625 Hi
I use TPS54625 for my VRM to x86 CPU. I want to make loop statility test on tps53625. There is some info on page 37 of the datasheet about the control loop, but the test point about the loop stability…
Part Number: TPS53625 Hello,
Customer change PR205 empty, PR208->10K / PR210->2K and increase 470uF cap. The specification of Closest and & Farthest DIMM are over DDR spread sheet 30mV as below. The low frequency transient response should be ok but…
Part Number: TPS53625 Hello,
Customer test intel spreadsheet. When output voltage decay to 0.64V on 10A, The alert not assert. Per spreadsheet, it needs to decay about 0.59 V the will send alert. But the output of TPS53625 can't decay more below 0.64V…