Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS53626 Other Parts Discussed in Thread: TPS53627 Hi,
Can you please help TPS53626 and TPS53627 schematic review?
If yes, attach it here? or send it by email?
Regards, Kevin.
Part Number: TPS53626 Other Parts Discussed in Thread: TPS53627 Hi,
My customer is currently desinging power blocks for VR13 using TPS53626 and TPS53627.
I have provided the excel-based calculation tool so that they can determine key component values. …
Part Number: TPS53626 Other Parts Discussed in Thread: TPS53355 Dear team,
Customer want to know resistor 30K and 39K are the same mode? What is the different when setting 30K or 39K?
Thanks.
Best regards,
Sammi
Part Number: TPS53626 Dear team,
Customer find two different calculation of equation in datasheet of TPS53626. Which one is the right equation for Icc(max)?
Thanks.
Best regards,
Sammi
Part Number: TPS53626 Dear Sir
TPS53626 we use in intel Denverton PVCCP specifications are as follows
Voltage Range=0.52~1.24V
Icc,tdc=18A
Icc,max=30A
OCP=50A
TOBvcc=+-25mV
LL=2.3mΩ
SVID ADDR=0x00H
We use 2 phase
Inductance specifications are as…
Part Number: TPS53626 Other Parts Discussed in Thread: TPS53627 , TPS53667 , TPS53679 , TPS53661 One of our customers chose TI power supply for the design.
Client proposal: Intel CPU is currently used for the product, and VR13.0 is required. Please refer…
Part Number: TPS53626 Other Parts Discussed in Thread: TPS53622 , TPS53625 Hi ,
If I use TPS53622 instead of intel Harcuvar CRB which has TI VR12 controller,
Does the platform BIOS or coreboot need to be reprogrammed for this new Vr13 change.
is there any…
Part Number: TPS53626 Hi team,
Refer to Table 11 in TPS53626 Datasheet, our customer choose ROCP=20kohm, but the test OCP value is still a littel large for them. So they're wondering if it's possible to connect a even smaller resistance to OCP pin to…
Part Number: TPS53626 Hi team,
I wonder the purpose of ICCMAX setting and OCP setting. As per the related thread, " The SVID bus has an alert triggering when Iout reaches ICCMAX (under normal operation it should not reach higher than ICCMAX), and…