Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS53626 Hi Team,
We've DIN TPS53626 in our customer, but they met dual pulse issue when doing frequency test of P1V2_VDDQ(connect to VFB pin), please refer to the waveform below, I can send you the schematic through email.
Test condition…
Part Number: TPS53626 Hi team,
I have questions in regard to the accuracy of pin-strap voltage range.
1. Setting Address thru the voltage on SLEWA pin
Customer is design Rtop 100k and Rbottom 39.2k, thereby the voltage on SLEWA pin is calculated as…
Hi Minkyung,
Usually there is mismatch between calculation and measurement due to component variation, board parasitic and etc.
I would suggest to tune compensation with bench test.
Thanks
Qian
Part Number: TPS53626 Hi,
I am reaching out for TPS53626 application. I want to know how to adjust DC gian to get better load regulaton. If anything is confidential, you can reply to jimmy-zhou@ti.com. Thanks!
Best regards!
jimmy-zhou ti.com.peter
Part Number: TPS53626 Hi there,
I wonder the inaccurate value setting on the pin-strapping can cause the fatal problem on operation. The designated ICC_MAX of the rail (by INTEL) is 9.7A and R_IMAX is supposed to be 3424.76 kOhm. But the customer uses…
Part Number: TPS53626 Dear All:
Has designed TPS53616 for intel platform C3000 VCCP power, Test load line slope 1.0mV/A, the datasheet remark 2.3mV/A, Debug CSP NET RES RCS(eff) , But have no effect;
debug RES Rcomp, can achieve 2.3mV/A, but the transient…