Part Number: TPS53689 Tool/software: Hello Team,
Currently my customer wants the FW with the requirement as below, can you help to share the FW? Thanks!
ChannelA output 4 phases, VOUT=0.58V, current 64A; Channel B output 2 phases, VOUT=0.7V, current…
Part Number: TPS53689 In TPS53689(step-down multiphase controller) datasheet
"Refer to the Technical Reference manual" sentence appears many times.
Where can I obtain documents?
Thanks
Part Number: TPS53689 How to define the spec for SVID Data input logic low ?
Is the input logic low less than 0.45V ? or have the other way to define spec ?
Part Number: TPS53689 for intel spreadsheet validation, we found that DVID slow down for 1V to 0.95V, t he output voltage have spike before dropping down.
How to improve it?
Part Number: TPS53689 Hi Team,
When the TPS53689 ACLL is set to be less than 0.125, it cannot be stored to the NVM, that is, it will return to 0.125 when powered on again. However, no errors were reported during this process. Is there a minimum value? …
Part Number: TPS53689 Team,
Customer is setting up TPS53689RSBR in system and would need to know these parameters that seems not stated in datasheet. Can you help to check and advise? Thanks.
(EE)_* Preheat/Soak Time between 150~200℃ (s) MAX:
…
Part Number: TPS53689T Other Parts Discussed in Thread: TPS53689 Tool/software: Hello,
Our customer has to program TPS53689T, but we support only TPS53689. It seems that there are some differences because device ID check doesn't pass. We need full device…