Part Number: TPS53689T Other Parts Discussed in Thread: CSD965200 , TPS537G2 , TPS53622 Tool/software: Hi,
We would like to generate up to 1000A of current for core power. Is it possible to recommend a reference design that can achieve this?
We used…
Part Number: TPS53689T Hi sir
we need a soluton which is pwm+TLVR, I would like to survye the TPS53689T
But no evb released, if you have other suggestion?
thanks
Part Number: TPS53689T Tool/software: Hello Team,
I am using TPS53689T VR14 IC, at pin 37 I have this voltage divider and pin 38 is connected to 12V.
When voltage at pin 37 is measured using multimeter, it is coming out to be 12V, whereas 1V is…
Part Number: TPS53689T Tool/software: Hello,
(1) I wanna ask which parameter and what value in TPS53689T's GUI as below we could fine-tune for VOUT shutdown during soft-start?
Or what are the other parameters you recommend for the issue?
(2…
Part Number: TPS53689T Other Parts Discussed in Thread: TPS536C9T Tool/software:
Hi All,
Good day ,
Our company is currently assessing the VR14 Compliant controller like the TPS53689T multiphase IC, thus the demand for TPS53689T VR14 controllers…
Part Number: TPS53689T
Tool/software:
Hi Team,
We are facing one issue with the TPS53689T controller.
When we are checking with CPU mounted on board, the system is going in S0 state and VRs are working correctly initially.
But, when the…
Part Number: TPS53689T Other Parts Discussed in Thread: CSD95410RRB , Tool/software: Hi
We're considering using the TPS53689T to generate a core voltage of 0.85V @ up to 300A with 6 phases (CSD95410RRB with "standard" power inductor) and utilizing the…