The title of your post subject is "TPS53915: find another DC/DC solution to generate 0.95V" but you are asking for a p2p to FP6385.
The TPS53915 is 4.5x3.5 12A device with PMBUS and the FP6385 sot-23 3.5A device.
I am going to change the subject…
Part Number: TPS53915 Other Parts Discussed in Thread: TPS549B22 , TPS548B22 Hi Team,
I am looking for a device which can support the following requirement:
1. Vin=2.5-5.5V
2. Vout=0.5V-1.2V, typical 0.6V
3. Iout_max=12A
I could see that TPS53915 can fulfill…
Part Number: TPS53915 Hi,
just realized the maximum voltage on the EN pin is stated to 7.7V in datasheet. We have been using using 10kOhm PU to 12V for multiple units for a few months now and just recently ordered new PBAs with the same design.
Any chance…
Part Number: TPS53915 Other Parts Discussed in Thread: TPS549A20 I was also looking another Device from TI "TPS53915RVER" as an alternate part of "TPS549A20RVER".
As i know TPS53915RVER is a 12A device, which is good enought for the…
Part Number: TPS53915 Hi experts,
The PCN# 20170804000C states a change in the material of the lead finish - NiPdAU (E4) and Matte Sn (E3)
2 questions:
a. Can customer used part# of both finishes inter-changably w/o making production line changes?
/cfs…
Part Number: TPS53915 Other Parts Discussed in Thread: TPS53513 , TPS53515 , TPS549A20 , TPS548A20 Hi,
Could TPS53915 as TPS53513 alternate source?
What's the circuit design different?
Part Number: TPS53915 Other Parts Discussed in Thread: TPS53515 Hi,
Can off-line programming TPS53915 to change FW setting before use.
For example, I would like to change TPS53915 frequency setting from 400kHz to 850kHz.
Thanks
Tony
Part Number: TPS53915 Other Parts Discussed in Thread: TPS53515 Hello Support team,
Since we are facing the delivery issue of TPS53515 now, we want to study TPS53915 as an alternative option.
Is it possible to apply TPS53915 instead of TPS53515 without…
Part Number: TPS53915 Hi expert,
My customer is validating the TPS53915, we are measuring the high side Vds waveform, please see condition below
Vin = 12V, Vout = 1.8V, with 10A, is this waveform reasonable or this fit our datasheet's spec? Cause we can…