Part Number: TPS5401 Following are our specifications:
Input Voltage Range: 6V to 24V
Output Voltage: 5V
Output Load Current: 0.1A
Created a snapshot of our design created in the web designer.
The crosses in the above design indicates the components…
Part Number: TPS5401 Good morning.
Received TPS5401DGQR of two different date codes and two different places of manufacturing - 1745 Made in China and 1823 Made in Thailand.
They bear two different types of manufacturer logo in top marking - the ones…
Part Number: TPS5401 Team,
regarding TPS5401DGQR, do you have any estimation what happens if VIN < -0.3V is applied?
I know this violates the abs max values and is out of spec, but is there any estimation for
part behavior and/or
expected kind of damage…
Part Number: TPS5401 Hi
Vout=12V and Iload=0.05A are assumed.
In customer design, when VIN is decreased around 15 V, output starts to lower than 12 V.
What do you think the cause of decreasing output level with decreasing input?
BestRegards
Part Number: TPS5401 We use it as per the following schematic, but are experiencing unreliability in terms of the achieved output voltage which should be 3.3Vdc and usually is, but other times can vary between about 2.7V and 3.6V (and this is tested with…
Part Number: TPS5401 Hi,
Please review the attached TPS5401 DC-DC converter design and please share your valuable comments on the same to improve the design,
I/p to the device is 4.5-32V and o/p is 3.3V/0.5A
Thanks
Part Number: TPS54040 Other Parts Discussed in Thread: TPS5401 , We are looking for a second source for TPS54040DGQ Requirements: Same as TPS54040DGQ 3.5V to 42V or more Input Voltage Range Min. 0.5 A Current limit PACKAGE 10 Pin MSOP
Can we take TPS5401?
Requirement…
Hi,
I did measurement on others board with different resistor values. Here are the results :
On the board #13 (with R1=100K and R2=8.2K) I measured the voltage between the pin EN and the ground. I found that the TPS5401 turn ON when the voltage on EN…
Part Number: TPS5401 Other Parts Discussed in Thread: TPS62175 Hello
My customer is evaluating TPS5401 for FY2018 audio product.
Attached is rough sketch of their schematic.
Anyway, customer want to control EN and RT/CLK.
Please let us know the recommended…
Part Number: TPS5401 Hello,
For the TPS5401, can we share the internal slope compensation values so the customer can design the rest of the circuit in accordance with those values?
Also, this application will require just under 600mA peak switch current…