Note that Cell A109 in the calculator tool for designing a positive-negative split-rail power supply is mislabled. It says "Copos" but should in fact say "Max Co ESR"
Part Number: TPS54260 Other Parts Discussed in Thread: TPS54360 , LMR36015 , LMR33630 , LMR33620 , LMR36006 Hi guys I am designing the power supply for a tracking device, which uses a GPRS and GPS module (MC60 from Quectel)
I am using TPS54360 with…
We are developing a high voltage charger. You can use similar ideas to build your high voltage charger. (See attached file)
Also, please see another related post.
http://e2e.ti.com/support/power_management/battery_management/f/179/p/60871/218590…
I split this thread since yours is a separate design from the original post.
I don't quite follow your description, so perhaps a waveform would better convey what you describe. In any case, I would recommend testing with the EVM as the layout can affect…
Hello Orlando,
I found one short circuit report in the TI website. in that, Short GND to PH mentioned - " Device is protected from overcurrent, but pass transistor may be damaged due to excessive heat. No Output"
Just I wanted to understand,
…
Other Parts Discussed in Thread: DRV8301 , TPS54160A My application for the DRV8301 integrated DC/DC requires a 5V output and operation from a large input voltage range (20-48V). Ideally, the DC/DC would be stable throughout the entire input voltage range…
I'm just playing around with SwitcherPro at the moment and one of the designs it came up with had multiple Schottky diodes in it. I presume these are supposed to be put in parallel and they're being suggested to meet the peak current requirements. Can…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…