Part Number: TPS54060 Hi Team,
Can you have a look at the following customer inquiry?
With the TPS54060, we experienced defective systems for which the static resistance between VIN and PH was low, looking like the internal FET switch was destroyed. What…
Other Parts Discussed in Thread: TPS54060A , TPS57060-Q1 I found that the junction temperatures for both is very different. It is way higher for the TPS57060-Q1 than the TPS54060A, this is because I need to replace the TPS54060A with the TPS57060-Q1, but…
Hi Henry,
Good Day. Please see below the response of our customer to your reply. Thank you very much.
I clearly noted that “ we can use the same TPS54540 to generate a negative output with an Inverting buck-boost (IBB) topology".
The problem…
Other Parts Discussed in Thread: TPS54160 Hi,
i have designed a DC-DC converter with input ranging from 8V to 48V and providing 5V output at 0.5A load current. Webench design suggested me a design which shows that top resistor used for UVLO condition is…
Part Number: TPS54060 Other Parts Discussed in Thread: , TINA-TI Before I find out the hard way, can you please tell me if the TINA-TI SPICE models for TPS54060 and TPS54060A support the inverting buck boost topology? Seems there are several device models…
Hi Ambreesh
Yes, it's clear that it only can regulate to 34V. I have TPS7A4901/TPS7A3001 devices behind it, but due to the assymetry, I get near to the drop-out voltage of a TPS7A4901 that is regulating to +16V.
But do you know what influences the…
Part Number: TPS54340 Other Parts Discussed in Thread: LM46001 , LM46000 , TPS54060A , TPS54160A , LMR16006 Hi,
I am considering an inverting circuit with the following specifications. There is PMP4369 in the reference design, but is it possible to adjust…
Hi Mr. Yang,
In order to get fast response, may I suggest you to start a new e2e thread under TPS54060A or TPS54360? Then, your question will be directed directly to the engineers supporting the buck as well as the inverting buck-boost applications…
Other Parts Discussed in Thread: TPS54531 , TPS54331 , TPS54060A Hello
Is it possible to use TPS54531 in negative configuration, to get -12V from +15V input?
I'd use another TPS54531 in parallel to get +12V from the same +15V.
If I didn't explain well…