Hi team,
I tried to perform the Load transient test as per the slvu299.pdf page no.6 sec 2.5 Load transients.
Load current steps are made as per the document.
But coming to measure AC coupled Output Voltage across C5, I observed more than 25mV of…
Part Number: TPS54060A Other Parts Discussed in Thread: TPS54060 , TPS54060EVM-457 Hi everyone, I am using the TPS54060 in a buck converter configuration, with an input voltage of 15V, an output voltage of 6V, and a maximum output current of 100mA. The…
Part Number: TPS54060EVM-590 Other Parts Discussed in Thread: TPS7A30-49EVM-567 , , TPS54060EVM-457 Hi TI team,
We bought TPS54060EVM-590 and tested with LDO TPS7A30-49EVM-567. They are working great!
Now we will integrate them two into our design…
Other Parts Discussed in Thread: TPS54060 , TPS54060EVM-457 Hello,
Two questions around the TPS54060:
1. To get a 39 V output from the TPS54060EVM-457, are there any other changes that need to be made besides the resistor divider R6/R7 (as shown in…
Other Parts Discussed in Thread: TPS54060 , TPS54060EVM-457 Hello,
we try to use the TPS54060 with 12V output voltage. In the datasheet the maximum output voltage isn't mentioned explicitely.
So we did a test with the TPS54060EVM-457 Evalboard.…