Part Number: TPS5410-Q1 Hi Team,
Customer wants to use TPS5410QDRQ1 as alternative for TPS5410DR due to current situation.
Could you give me comment on following customer questions?
1. Are there any differences between TPS5410DR and TPS5410QDRQ1in terms…
Part Number: TPS5410 Hello Expert,
Our customer has a symptom that there is Vout drift issue between feedback resistors.
Below is my questions.
Could you please reply to my each question?
1. When I checked recommended Rfbt resistor on the data sheet and…
Part Number: TPS5410-Q1 Hello ,
I am currently using TPS5410-Q1 on a PCB , My objective is to get a variable DC-DC Conversion with an input of 24V to an output that varies between 7 to 17V , I added a Digital Potentiometer (U5) instead of the bottom resistor…
Part Number: TPS5410 Hi,
I am facing the same issue(Same wave form) like in the below link.
https://e2e.ti.com/support/power-management/f/power-management-forum/443019/tps5410-startup-problem
What could be the reason for this issue? Is there any solution…
Part Number: TPS5410-Q1 Other Parts Discussed in Thread: TPS5410
Q1) What is the approximate open load ENA voltage when VIN is 13.5V?
Q2) Do I need a diode from ENA to VIN to protect ENA pin (from 100uF cap on the pin) if VIN drops suddenly?
Q3) Is slow…
Part Number: TPS5410 Hi TI Team,
Actually, our design is for Solar tracking system. The main power source is from State board grid power source. That grid power goes to an inverter and then AC-DC Meanwell Power supply (RS-100-24). AC-DC will generate…
Part Number: TPS5410-EP Other Parts Discussed in Thread: TPS5410 , Hi,
Can you provide the thermal parameters (Psi, Theta) for the TPS5410?
Is there some web page or app note which contains this information for common TI packages?
Thanks
Part Number: TPS5410 Tool/software: WEBENCH® Design Tools Hello,
I have downloaded TPS5410 un-encrypted average model from TI website & ran the un-encrypted model in OrCad PSpice 16.6. Does this model work in CCM only or it auto-toggles between CCM…
Part Number: TPS5410 Team,
In the area circled be low, not for efficiency but for ripple. If I operate in that region will I be putting the part in discontinuous mode? What will the ripple look like?
Part Number: TPS5410 Hi Team,
One of my customer is using TPS5410 in their application. Vin=12V, Vout = 5V. The load conditions are 35mA and 200mA (switching between the two loads). The ripple at 35mA is very high, where as with load of 200mA the output…