Part Number: TPS5410
As title, I have 3 question.
First , please look at picture.
If the TPS5410 output is 5 Voltage,I need to control the ripple value at 3-5%;May be is 150mV-250mV(ideal)
But i find the TPS5410 oringinal EVM Board,which output is for…
Hello , recently I am busy , so i didn't reply at first timed. before u reply me from Nov 16, 2018 1:32 AM. i have test the 2 vesion of circuit. like the picture
the v1 is input cap and inductor close to tps5410
the v2 is input cap , output cap…
Part Number: TPS5410
hello guys , i have confuse on this question ,
that i measure the tps5410 output ripple by use difference bandwith
one is 200mhz like picture for this
another is like this
bandwith is 20mhz
on ti office has video to teach measure…
Part Number: TPS5410 Hi,
What is the Iout current needed to be considered for the Lmin calculation of TPS5410
When we are considering Iout max (500mA) the Lmin is 40uH
Inom is 300mA . So the Lmin is 67uH. Iout Min is 250mA. So Lmin =80uH
So for the Lmin…
Part Number: TPS5410 Hi Guys , I have use TPS5410-EVM board , and that is good Perfect waveform and good ripple .
But i designe the new circuit for tps5410 which cap and resistor is choice by myself.
then the circuit is like this.
Now i have problem…
Part Number: TPS5410-Q1 This circuit attached is conducting 100MHz noise back onto the power input line. Attached is the circuit and the radiated EMC trace. 676750 Rev C_Logic0.pdf
Part Number: TPS5410 Hi,
I have used TPS5410 for 12V to 5V DC-DC converter.
Load - 50mA to 220mA(Toggling)
Lmin for 220mA = 98H(100H used)
So at Load of 220mA 5V , ripplw is negligible. But at 50mA ripple is around 200mV.
When the load is changing from…
Part Number: TPS5410-Q1 Other Parts Discussed in Thread: TPS5410 I am doing a redesign for a production ECU to replace obsolete parts and I chose the TI TPS-5410 regulator to save complexity and reduce some of the switching noise on the prior design. However…