Part Number: TPS54160 Other Parts Discussed in Thread: TINA-TI Hello guys,
One of my customers is trying to simulate TPS54160 load transient using TINA-TI. The attached file is their schematic. But TINA-TI transient simulation didn't run with this file…
Part Number: TPS54160 Hello, I read Experiment Buck and have been doing experiment using it.
While measure efficiency of TPS54160, I found something strange.
I have two questions.
First question,
In datasheet of TPS54160, the efficiency curve…
Part Number: TPS54160 Hi Team,
1. When the RT resistance is 390K, it is found that the 3.3V output is abnormal. After powering on, 3.3V will be pulled down to 1V.
2. If the RT resistor 390K change to 90.9K, this output voltage will be 3.3V.
Part Number: TPS54160 Hello guys,
One of my customers has been using TPS54160DGQ for their mass-production.
Recently, they received PCN of the device (PCN# 20230928002.1). The PCN says that new assembly site, HFTF was added and qualified. Also it…
Part Number: TPS54160 Hi TI support team!
We are using EVkit of TPS54160 for load transient experiment in the laboratory component of switched-mode power conversion course. Due to the pandemic we have moved on to having online simulation based experiment…
Part Number: TPS54160 Hi
I am trying to investigate how to calculate appropriate capacitor and resistor values (C1, C2 and R3) for a type 2A compensation circuit described in the datasheet on page 29 and started looking at the formulas on page 30. …
Part Number: TPS54160 Hi,
I got this part with mismatch thermal pad dimension against the drawing. Is this OK?
It is even less than the thickest stencil recommended design. I wonder if this might cause solder overflow?
Thanks,
Ireen
Part Number: TPS54160 Dear TI,
according to datasheet of TPS54160, absolute maximal current via PWRGD (power good) pin is 10 mA.
Datasheet section 8.3.17 Power Good (PWRGD Pin) describes: The PWRGD is in a defined state once the VIN input voltage…