Part Number: TPS54160A Other Parts Discussed in Thread: TPS54160 ,
Tool/software:
Hi, I'm using the TPS54160ADRCR as an inverting pwr supply, from +24V to -6V following the SWIFTINV-CALC-REVE.xls excel sheet and the SLVA317B document instructions…
Part Number: TPS54160A Tool/software: I need to model TPS54160A using 4-element VRM model with the parameter of slew inductance(Lslew), Flat Resistance(Rflat), Output inductance (Lout), Output Resistance(Ro). Could you suggest how to calculate the parameters…
Part Number: TPS54160A Tool/software:
I'm confused by the power good operation when running TPS54160A with a negative output voltage. I would have assumed that power good be de-asserted because the VSENSE-GND votlage is 0.8V. It's just that GND is at…
Part Number: TPS54160A Tool/software: I've been designing power converters using the TPS54160ADRCR but I've noticed that the inductor calculation on page 32 of the datasheet only specifies the output current, not a minimum or maximum. I've noticed in…
Part Number: TPS54160A
Tool/software:
Hi team,
A new DGQ package has been added, but the PAD dimensions are different. Would it be appropriate to make the opening 1.75x1.89mm so that it can accommodate either package? Is it possible to specify either…
Part Number: TPS54160A Hi,
I'm using TPS54160A since 10 years in many different designs, multiple ICs for different voltages. Since some months there is an increase in blown up ICs in series production. I cannot remember ever having problems with this…
Part Number: TPS54160A Hello team,
My customer is observing current limit operating at lower current level than datasheet spec.
The minimum current limit is 1.8A on the datasheet, but customer has observed at 1.6A on their board.
The operating…
Part Number: TPS63000 Other Parts Discussed in Thread: TPS54160 , TPS54160A Dear TI team of experts. We have an unexpected behaviour in the series production of one of our PCBs. After some time, the output voltage of the two DC/DC converters starts to…
Part Number: TPS54160A How is relationship between VIN and VOU
for example, i want to design a circuit that OUTPUT is 6V .
The VIN minimum is 6+(voltage reference 0.8)=6.8V right?