Part Number: TPS541620 Hi team,
This has a good chance to make it into on if my customers designs, but they are trying to move fast and their favorite way to quickly sim is with webench. I guess the dual output makes that tough with the Webench interface…
Part Number: TPS541620 Other Parts Discussed in Thread: TPS53820 Hi team,
Could you please help me to pick up multi-sourcing availabe dual phase converter?
The requirement is Vin=12V,Vout=0.8V,Iout>=12A.
We've been promoted TPS541620, but it doesn…
Part Number: TPS541620 Other Parts Discussed in Thread: TPSM5D1806 I am looking for voltage regulator preferably Linear regulator for my design. My input voltage range is 5V-10V (coming from benchtop DC power supply).
I need to supply four different voltages…
Part Number: TPS541620 Hi Team,
My customer is in layout of TPS541620, but the package size info is missing in datasheet.
Could you provide the info to help customer layout or provide the device PCB library (AD/Cadence or others should be OK).
Thank you…
Part Number: TPS541620 Hi team,
Could you help to provide the cost-optimized replacement for LTC3636? I think TPS541620 could be one of the option.
Thanks.
If I remember correctly, the SS and RS- pins mux'ed out of the circuit to use internal circuit or a node. So I cant think of a way to use these pins.
FYI, the TPS541620 is the converter used on TPSM5D1806.
Part Number: TPSM5D1806 Other Parts Discussed in Thread: TPS541620
Hi All,
The Device TPSM5D1806 has a pin called BP5 which as per the data sheet is a 5 V nominal (Range = 4.8 V to 5.2 V) regulated output.
My question is :
If I use Vin = 5 V, can the…
Kian
First, 12V @ 45W is not going to provide the input power necessary to source 16x 4.3V @ 1A (68.8W) of output power, so your sourcing supply could be an issue. I would recommend a minimum of a 75W supply for powering 16x 4.3V @ 1A
Second, TI offer…