Part Number: TPS5430 Other Parts Discussed in Thread: TPS5420 , , TPS54202 Dears
It is said that TPS54X0 is not recommand for new design, Could you help to tell us why?
If not recommand which parts could replace them.such as TPS5420 TPS5430 and so on.
Part Number: BQ25892 Other Parts Discussed in Thread: TPS5420 , BQSTUDIO
Hi,
I have a small design with a GSM module and I use as power management the BQ25892 chip.
The design input voltage is regulated using a TPS5420 converter with the output set at…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS5420-Q1 , TPS54560-Q1 , LM76003 , LM73606 We are using TPS54260-Q1 Automotive qualified DC DC converters in our existing design.
But we do face EMI/EMC issues on 2 layer PCB boards.
So we require…
Hi Venter,
The datasheet did not specify the exact condition when the hiccup behavior is triggered. It is hard to get around it. Would you try to use TPS5420 instead? TPS5420 is pin to pin compatible with TPS5410 and has twice current rating.
You can…
Thank you for your answer!
I understood that LM25005 does not have PFM mode.
And we think that TPS5420 does not have PFM mode(light load mode).
Is the above recognition correct?
Best regards,
Takahiro Nishizawa
Part Number: TPS5450-Q1 Other Parts Discussed in Thread: TPS5420 , TPS5450 Tool/software: WEBENCH® Design Tools Hello,
We've been using the TPS5420 successfully in various designs but need to move to the TPS5450. We are having trouble getting stable…
Hi Nirav,
the board is based on the tms320f28377s device, in particular we referred to the LAUNCHXL-F28377S. We decided to put on the board only the JTAG connector and use the XDS110 probe for test and program activities.
The board will be used as controller…
Other Parts Discussed in Thread: TPS5420 , ADS5400 Hello,
last week I burned TPS5420 regulator on ADS5400 evaluation board. The manual states that "the input power supply voltage range for the EVM can be 6 V to 36 V only if the onboard TI power solution…
Other Parts Discussed in Thread: LM3480 , TPS5420 Attached is my schematic. This is an automotive IoT device that will connect to the headers on a raspberry Pi. It will sniff the can bus on Semi Trucks and collect data from the internal controllers and…
Other Parts Discussed in Thread: TPS5410-Q1 , TPS5430-Q1 , TPS5420 , TPS5410 , TPS5430 , TPS5420-Q1 Hello,
I am having trouble with the TPS5410-Q1 not starting with a load applied. Please see the description below.
Thank you in advance for your help.
Schematic…