Part Number: TPS5420-EP Hi Team,
I am using TPS5420MDREP power converter. The input voltage will vary from 17V to 35V, below 17V the device should shutdown so that is UVLO. So can I use resistor divider on ENA pin from the input like R1=330K and R2…
Part Number: TPS5420-EP
Hello ,
We have a need on the TPS5420-EP (10.000 PCEs / Year), but before we need more technical informations about the BiCMOS LBC4 BOA process technology :
-The feature size : 0.35 µm , 0.32 µm ??
-The substrate : SOI…