Part Number: TPS54202H Hi team,
below is customer schematic and layout, their input is 13.5V,output is 2.8V/175mA
customer found the output ripple is too large which can't meet their requirement. now the output ripple is 50mV, they require ripple should…
Part Number: TPS54202H Other Parts Discussed in Thread: TPS54202 The maximum voltage of the enable pin is specified 7V in the datasheet, but at your evaluation board it is connected to the input which can even be 28V. Can this pin handle this higher voltage…
Part Number: TPS54202 Hello team,
I'd like to confirm the differences between TPS54202 vs TPS54202H.
From my understanding,
1: The device has SSC or not.
2: The device has an internal pull-down 1Mohm or not.
and EN hysteresis current looks different…
Part Number: TPS54202H Other Parts Discussed in Thread: TPS54302 Hello guys,
One of my customers is considering using TPS54202H for their next products.
They found the following description on page 11 in the device datasheet (SLVSDG7).
"7.3.11 Bootstrap…
Part Number: TPS54202H We are designing a 3.3V power supply with the TPS54202H and an average current of ~1A.
During 300mA load step (that happens regularly) we see a voltage swing lasting for 100µs. Adding a feed forward capacitor, we are able to reduce…
Part Number: TPS54202H Other Parts Discussed in Thread: TPS56339 Hi sir,
Please kindly help to suggest the solution to replace MP2314.
P-P compatible would be nice, thanks a lot!
Best Regards,
Sean Liao
Part Number: TPS54202H Other Parts Discussed in Thread: TPS562201 , TPS54202 Hello,
I am trying to configure TPS54202H for 12V output (max current 1.5A).
The problem:
As soon as a power source is connected to the input, the part fails and the input get…
Part Number: TPS54202H Other Parts Discussed in Thread: TPS54202 Hi All, I use TPS54202H as a 12V to 3.3V converter with a small load of 100mA and a peak of about 500mA (MCU, WiFi module, LoRa module). On the same bus of 12V another TPS54202H is used to…